LPC11U34F not responding - Cannot provide power to DAP bus.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC11U34F not responding - Cannot provide power to DAP bus.

1,207 次查看
SamiG
Contributor I

Hello, I am trying to debug the firmware for a custom board using the LPC11U34F, using the MCU-LINK debugger. It worked fine for three tries, then stopped working.

When I try to debug, I get the following errors:

Error 1:

Pasted File at December 15, 2021 6_35 PM.png

"Failed to execute MI command:

-target-select extended-remote | crt_emu_cm_redlink -msg-port=1093 -g -mi -2 -pLPC11U14/201 -vendor=NXP --reset= -ProbeHandle=1 -CoreIndex=0 --flash-hashing --flash-driver LPC11_12_13_32K_4K.cfx --telnet 3333

Error message from debugger back end:

Remote communication error. Target disconnected.: No error.

Failed to execute MI command:

-target-select extended-remote | crt_emu_cm_redlink -msg-port=1093 -g -mi -2 -pLPC11U14/201 -vendor=NXP --reset= -ProbeHandle=1 -CoreIndex=0 --flash-hashing --flash-driver LPC11_12_13_32K_4K.cfx --telnet 3333

Error message from debugger back end:

Remote communication error. Target disconnected.: No error."

Error 2:

Pasted File at December 15, 2021 6_36 PM.png

Error 3:

Pasted File at December 15, 2021 6_37 PM.png

"02: Failed on connect

02: Failed on connect

Cannot provide power to DAP bus.

Probe(0): Connected&Reset. Was: NotConnected. DpID: 0BB11477. CpuID: 00000000. Info: <None>

Debugging context: nxp_lpcxpresso_11u14_periph_blinky LinkServer Debug

Failed on connect: Em(04). Cannot provide power to DAP bus.

Connected&Reset. Was: NotConnected. DpID: 0BB11477. CpuID: 00000000. Info: <None>

Last stub error 0: OK"

I can't erase the firmware using Flash Magic either.

Do you have any suggestions or questions?

Thank you for your time!

标签 (1)
0 项奖励
回复
1 回复

1,168 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Please try follows:

1. create a new workspace

2. create a new project under this workspace

3. the board connects computer in ISP mode

4. try debug

How does it work?

If still fails, reinstall MCU-Link driver with this guide then do step 1-4 again.

https://www.nxp.com/document/guide/getting-started-with-the-mcu-link:GS-MCU-LINK

 

Hope this helps,

Jun Zhang

0 项奖励
回复