LPC11U14 as USB host

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC11U14 as USB host

1,977 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tuv0k on Sun Mar 09 16:56:56 MST 2014
Is it possible for LPC11U14 to operate in USB Host mode and connect the i.e. hid device to it?
Labels (1)
0 Kudos
Reply
3 Replies

1,959 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tuv0k on Tue Mar 11 00:11:32 MST 2014
Thanks guys, I figured it out. I can use uC from LPC17xx series :)
0 Kudos
Reply

1,959 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by usb10185 on Mon Mar 10 15:21:25 MST 2014
These parts only supports FS Device mode so it will act nicely as a HID Device.

Have a look here for USB Host and Device parts from NXP
http://www.lpcware.com/content/project/nxp-peripherals/usb-nxp-microcontrollers
0 Kudos
Reply

1,959 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mattes on Mon Mar 10 11:23:14 MST 2014
I am using 11U14 in device mode, which is using the software usb stack, which is supporting
USB host mode.    See http://docs.lpcware.com/nxpusblib/v0.98/index.html for more details.

From a software point , yes the host mode is available. So far I did not see any limitation why
the 11U14 would not support it. 
0 Kudos
Reply