LPC11E1X Transistor size?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC11E1X Transistor size?

ソリューションへジャンプ
2,115件の閲覧回数
haydenw
Contributor I

I'm using the LPC11E14 in a project and I was just wondering what the transistor process size of this microcontroller is? Is it documented somewhere?

タグ(1)
0 件の賞賛
返信
1 解決策
2,108件の閲覧回数
converse
Senior Contributor V

This is not normally something that is publicised. However, I seem to remember that LPC11 is based on 130nm process (LPC18/43 is 90nm). The limiting factor for microcontrollers is flash.

 

元の投稿で解決策を見る

2 返答(返信)
2,109件の閲覧回数
converse
Senior Contributor V

This is not normally something that is publicised. However, I seem to remember that LPC11 is based on 130nm process (LPC18/43 is 90nm). The limiting factor for microcontrollers is flash.

 

2,099件の閲覧回数
haydenw
Contributor I

Yeah okay it seems like I would have to contact NXP directly to get that information, thanks anyway for your insight.

0 件の賞賛
返信