LPC11E1X Transistor size?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC11E1X Transistor size?

跳至解决方案
2,127 次查看
haydenw
Contributor I

I'm using the LPC11E14 in a project and I was just wondering what the transistor process size of this microcontroller is? Is it documented somewhere?

标记 (1)
0 项奖励
回复
1 解答
2,120 次查看
converse
Senior Contributor V

This is not normally something that is publicised. However, I seem to remember that LPC11 is based on 130nm process (LPC18/43 is 90nm). The limiting factor for microcontrollers is flash.

 

在原帖中查看解决方案

2 回复数
2,121 次查看
converse
Senior Contributor V

This is not normally something that is publicised. However, I seem to remember that LPC11 is based on 130nm process (LPC18/43 is 90nm). The limiting factor for microcontrollers is flash.

 

2,111 次查看
haydenw
Contributor I

Yeah okay it seems like I would have to contact NXP directly to get that information, thanks anyway for your insight.

0 项奖励
回复