LPC11E1X Transistor size?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC11E1X Transistor size?

Jump to solution
2,081 Views
haydenw
Contributor I

I'm using the LPC11E14 in a project and I was just wondering what the transistor process size of this microcontroller is? Is it documented somewhere?

Tags (1)
0 Kudos
Reply
1 Solution
2,074 Views
converse
Senior Contributor V

This is not normally something that is publicised. However, I seem to remember that LPC11 is based on 130nm process (LPC18/43 is 90nm). The limiting factor for microcontrollers is flash.

 

View solution in original post

2 Replies
2,075 Views
converse
Senior Contributor V

This is not normally something that is publicised. However, I seem to remember that LPC11 is based on 130nm process (LPC18/43 is 90nm). The limiting factor for microcontrollers is flash.

 

2,065 Views
haydenw
Contributor I

Yeah okay it seems like I would have to contact NXP directly to get that information, thanks anyway for your insight.

0 Kudos
Reply