LPC11E14 - How to execute program using ISP command

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC11E14 - How to execute program using ISP command

3,633 次查看
masterboy
Contributor III

Hi all,

I need advice on what is the correct command to start the program via ISP. I tried the "G 0 T" and "G 512 T", but neither command my program does not start.

I tried a program Flash Magic, which is a function to start the program. When I set it up as follows (see figure), program starts ... I have a feeling that the program Flash Magic is doing something other than specified in the UM.155767_155767.pnggo.png

标签 (1)
标记 (4)
0 项奖励
回复
3 回复数

3,383 次查看
masterboy
Contributor III

I have a program with which the MCU upload the program (ISP mode). After loading the program I need to make the program started, but can be reset via the MCU pin.

For LPC1114 command "GO 0 T" works, but LPC11E14 not.

0 项奖励
回复

3,383 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Master Boy,

In which address is your reset code loaded? The GO command should point to the reset handler and must be used with an address of 0x0000 0200 or greater.

Thanks in advance for your response!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 项奖励
回复

3,383 次查看
martin_maurer
Contributor III

Do you just want to start your freshly loaded firmware? How about to pull reset (if available)?

If the above execution inside Flash Magic is working, have you taken into account, that vector table is used?

Is does not jump to position 0 but look at address 0 (or was it 4? One was Stack Pointer, one was Start Address)

where it shall jump to.

0 项奖励
回复