LPC11C24 using SSP1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC11C24 using SSP1

2,719件の閲覧回数
sukkinpang
Contributor I

I'm using the LPC11C24 and it has been successful on SSP0. Now I want to use SSP1 is well. I've set the PinMux to:

 

Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO2_2, (IOCON_FUNC1 | IOCON_MODE_INACT));// MISO1
Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO2_3, (IOCON_FUNC1 | IOCON_MODE_INACT));// MOSI1
Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO2_0, (IOCON_FUNC1 | IOCON_MODE_INACT));// SSEL1
Chip_IOCON_PinMuxSet(LPC_IOCON, IOCON_PIO2_1, (IOCON_FUNC1 | IOCON_MODE_INACT));// SCK1

#define LPC_SSP           LPC_SSP1

 

Using the same code for the SSP0 and with a scope on SSEL1 and SCK1 I can't see any signals.

 

Is there anything else that need to be configured for use with SSP1?

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,468件の閲覧回数
sukkinpang
Contributor I

Adding  | 0xC0 didn't help. Checking SYSCON.PRESETCTRL.2 is not easy as everything is abstracted, I'm using the npx_lpcxpresso_11c24_periph_ssp example.

I just changed the #define LPC_SSP    LPC_SSP0 to   #define LPC_SSP           LPC_SSP1

and changed the pinmux setting.

I have found this SSP1 example to be working. It uses these settings

    //SET UP THE SPI

    LPC_IOCON->PIO2_3          = (LPC_IOCON->PIO2_3 & ~(0x3)) | 0x2;   //set PIO2_3 up as MOSI function (sec. 7.4.34)

    LPC_IOCON->PIO2_2          = (LPC_IOCON->PIO2_2 & ~(0x3)) | 0x2;   //set PIO2_2 up as MISO function (sec. 7.4.22)

    LPC_IOCON->PIO2_0          = (LPC_IOCON->PIO2_0 & ~(0x3)) | 0x2;   //set PIO2_0 up as SSEL function (sec. 7.4.2)

    LPC_IOCON->PIO2_1          = (LPC_IOCON->PIO2_1 & ~(0x3)) | 0x2;   //set PIO2_1 up as SCK function (sec. 7.4.9)

    LPC_SYSCON->SYSAHBCLKCTRL  |= (1<<18);                             //enable clock to SPI1 block (sec. 3.5.14)

    LPC_SYSCON->SSP1CLKDIV     |= 0x2F;                                //enable SPI clk by writing non-zero clk divisor (sec. 3.5.17)

    LPC_SYSCON->PRESETCTRL     |= 0x04;                                //clear SPI reset, SPI held in reset by default (sec. 3.5.2)

    LPC_SSP1->CR0              |= 0x07;                                //set for 8 bit transfer (sec. 14.6.1)

    LPC_SSP1->CR1              |= 0x02;                                //enable SPI (sec. 14.6.2)

The trouble is, this project is based on the CMSIS and I can't put the above code in the lpcexpresso project. It won't compile.

Can someone please try the npx_lpcxpresso_11c24_periph_ssp example on SSP1.

0 件の賞賛
返信

2,468件の閲覧回数
rolfmeeser
NXP Employee
NXP Employee

Double-check that the SSP1 is not in reset mode (SYSCON.PRESETCTRL.2)

Make sure the clock divider for SSP1 is set to a non-zero value in SYSCON.SSP1CLKDIV

Try adding 0xC0 to the mode bits (as in  (IOCON_FUNC1 | IOCON_MODE_INACT | 0xC0) )

0 件の賞賛
返信