LPC11C24 can unused port pins be set and cleared

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC11C24 can unused port pins be set and cleared

跳至解决方案
1,039 次查看
steve_stone
Contributor I

I am using a LPC11C24 and was wondering if the unused port pins (PIO1_9 or PIO2_4 or PIO2_5 or PIO2_5) can still be set up as outputs an set or cleared and read back....wanting to use them as a bit of memory to enable or disable running secondary boot loader.

Thanks,

Steve

标签 (1)
0 项奖励
回复
1 解答
958 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Steve Stone

For the unused non-open-drain IO, it can be left unconnected if driven LOW and configured as GPIO output with pull-up disabled by software.

For the unused open-drain IO, it can be left unconnected if driven LOW and configured as GPIO output by software.

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
959 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Steve Stone

For the unused non-open-drain IO, it can be left unconnected if driven LOW and configured as GPIO output with pull-up disabled by software.

For the unused open-drain IO, it can be left unconnected if driven LOW and configured as GPIO output by software.

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复