LPC11C24 - UART configered as RS485 or RS232

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC11C24 - UART configered as RS485 or RS232

949 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rc51 on Thu Oct 23 07:44:13 MST 2014
The documentation discusses UART being used for RS485 -

If we want to use this as RS232 - can it be used for this?  Is there an app note or example project I can refer to?  Thank you.
标签 (1)
0 项奖励
回复
3 回复数

834 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Fri Oct 24 07:42:04 MST 2014

Quote: rickcartier51
I see - just need to use an external RS232 phy/driver.



Yes, a 3V version like MAX3232...

http://pdfserv.maximintegrated.com/en/ds/MAX3222-MAX3241.pdf
0 项奖励
回复

834 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rc51 on Fri Oct 24 07:19:03 MST 2014
I see - just need to use an external RS232 phy/driver.

Thank you.
0 项奖励
回复

834 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Thu Oct 23 07:49:38 MST 2014
Of course you can use it as RS232...

LPCOpen Samples:

http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc11xx-packages-0
0 项奖励
回复