LPC11C24 - Second bootloader and target application with CAN phy support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC11C24 - Second bootloader and target application with CAN phy support

834 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bomba82 on Wed Feb 05 02:24:23 MST 2014
After opening a thread for HardFault problems caused by CAN phy, I think that I have to know something in advance.

Does someone know if it's possible to develop a target application with CAN phy support, that can be deployed to the device via a second bootloader with CAN phy support?
I think my second bootloader is already ok, but I can't have success in developing a running target application. As I can understand the problem is that the CAN ISR is the cause of some kind of problem.

Can someone from NXP tell if it's impossible to implement that solution? And in that case, what's the reason?
Labels (1)
0 Kudos
Reply
0 Replies