LPC11C14 SPI configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC11C14 SPI configuration

4,084件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Detli on Thu Dec 19 07:58:14 MST 2013
Hello,

i have a problem with the spi unit and i hope there is someone who can help me! :-)

I like to read data from an ADC with 24 MHz.
I use the internal RC oszillator with the pll for 48 MHz.
So i adjust the spi registers, but whenn i measure the spi clock with an oscilloscop, i measure only 12 MHz Clock.
Maybe i have a fault in my code?

###################################################

From system_LPC11xx.c :

#define CLOCK_SETUP           1
#define SYSCLK_SETUP          1
#define SYSOSC_SETUP          1
#define SYSOSCCTRL_Val        0x00000000
#define WDTOSC_SETUP          0
#define WDTOSCCTRL_Val        0x00000000
#define SYSPLLCLKSEL_Val      0x00000000
#define SYSPLL_SETUP          1
#define SYSPLLCTRL_Val        0x00000023
#define MAINCLKSEL_Val        0x00000003
#define SYSAHBCLKDIV_Val      0x00000001
#define AHBCLKCTRL_Val        0b0011011111111111111
#define SSP0CLKDIV_Val        0x00000001
#define UARTCLKDIV_Val        0x00000001
#define SSP1CLKDIV_Val        0x00000001

####################################################

From my main.c :

//SPI0
LPC_SYSCON->PRESETCTRL|= 0x01;//Reset De-Assert SPI0
LPC_SYSCON->SSP0CLKDIV|= 0x01;//Clock Divider = 1

//MISO
LPC_GPIO0->DIR&= ~(1<<8);
LPC_IOCON->PIO0_8|= 0x01;
//MOSI
LPC_GPIO0->DIR|= (1<<9);
LPC_IOCON->PIO0_9|= 0x01;
//CLK
LPC_IOCON->SCK_LOC|= 0x02;
LPC_GPIO0->DIR|= (1<<6);
LPC_IOCON->PIO0_6 |= 0x02;
//CS
LPC_GPIO2->DIR|= (1<<8);
LPC_IOCON->PIO2_8|= 0x10;
LPC_GPIO2->DATA|= (1<<8);

//Serial Clock Rate = PCLK / ( CPSDVSR*(SCR+1) ) ; SCR=0 ; PCLK=48MHz ; CPSDVSR=2 ;
//LPC_SSP0->DR = Data Register to write
LPC_SSP0->CPSR|= 0x02;//CPSDVSR = 2
LPC_SSP0->CR0 = 0x00;
LPC_SSP0->CR0|= 0x18f;//16bit Transfer ; SPI Format ; CLK Low between Frames ; SCR = 1

uint8_t i;
for ( i = 0; i < 8; i++ )
{
     spi_data = LPC_SSP0->DR;    //Tab 210 clear the RxFIFO
}

NVIC_EnableIRQ(SSP0_IRQn);    //Tab 442
LPC_SSP0->CR1|= 0x02;//SPI Enable

#############################################################
ラベル(1)
0 件の賞賛
返信
10 返答(返信)

3,924件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 1234567890 on Mon Dec 23 05:29:41 MST 2013

Quote: R2D2

If you want to write 2 frames, you shouldn't toggle CS meanwhile...



Have you tried this?
- CS low
- for-loop
- CS high
0 件の賞賛
返信

3,924件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Detli on Fri Dec 20 12:34:31 MST 2013
Have no one a answer?
0 件の賞賛
返信

3,924件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Detli on Thu Dec 19 23:02:06 MST 2013
First of all, thanks for your help! :-)

I  hope it is a problem of the code. But it is possible, that the SPI Unit takes minimum 1,5 µS before it can receive a new frame?
If its true, than I have a real problem!

At the moment, the sending time for 16 bit  is about 700ns [ (1/24MHz )*16 = 666,67ns ].
Than there is a pause for 800ns before the next receiving starts.
Why is this break so long? I know there must be a little time between the frames, but that should not so long? I have tryed it with the code that was posted yesterday. I found no new knowledge in the example..

Many thanks
0 件の賞賛
返信

3,924件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Thu Dec 19 10:47:08 MST 2013
BTW: There's a SSP sample in NXP_LPCXpresso11C24_2011-01-27.zip.

If you want to write 2 frames, you shouldn't toggle CS meanwhile...

0 件の賞賛
返信

3,924件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Detli on Thu Dec 19 09:45:18 MST 2013
Yes, it works as master!

#####################################################
global:

uint8_t i = 0;
uint16_t Signal[100];

######################################################

main:

for(i=0;i<100;i++)
{
      spi_receive();
}//for

######################################################
void spi_receive()
{
//CS Low
LPC_GPIO2->MASKED_ACCESS[(1<<8)] = 0;

LPC_SSP0->DR = 0xff;//Dummy
while( ( LPC_SSP0->SR&(1<<4) ) ); //Wait until BUSY Bit clear

        //CS High
LPC_GPIO2->MASKED_ACCESS[(1<<8)] = ~0;

Signal = LPC_SSP0->DR;//Read Value
}//spi_receive()
0 件の賞賛
返信

3,924件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Thu Dec 19 09:40:46 MST 2013

Quote: Detli
I will explain :-)

The time between two 16 bit frames is to long.



This are frames which are generated from LPC11C14 as master?

Could be useful if you post this part of your code....


0 件の賞賛
返信

3,924件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Detli on Thu Dec 19 09:21:28 MST 2013
I will explain :-)

The time between two 16 bit frames is to long.
When I will receive frames directly behind on another, than the time between them is so long like the receiving time.
The break between them should not exist.

I hope you can understand my problem now.
0 件の賞賛
返信

3,924件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Thu Dec 19 09:15:12 MST 2013

Quote: Detli
The time between two receives is to long...



No idea who receives what here  :quest:
0 件の賞賛
返信

3,924件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Detli on Thu Dec 19 09:03:21 MST 2013
Thank you for the hint and the fast reply!

But I have already changed this to:
 
     LPC_SSP0->CR0 |= 0x8f;

and then, i measured it with my oscilloscop. Here was the fault, the parasitary capacitance of the probe had changed the signal -.-

Thank you ! It works now correctly ! :-)

But there is another problem!

The time between two receives is to long, i can get only 800kHz and not 1,5MHz (24MHz / 16bit).
Maybe you have a solution for this problem?
0 件の賞賛
返信

3,924件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Thu Dec 19 08:10:53 MST 2013

Quote: Detli
Maybe i have a fault in my code?



Yes.


Quote: Detli


//Serial Clock Rate = PCLK / ( CPSDVSR*(SCR+1) ) ; SCR=0 ; PCLK=48MHz ; CPSDVSR=2 ;
//LPC_SSP0->DR = Data Register to write
LPC_SSP0->CPSR|= 0x02;//CPSDVSR = 2
LPC_SSP0->CR0 = 0x00;
LPC_SSP0->CR0|= 0x[color=#f00]1[/color]8f;//16bit Transfer ; SPI Format ; CLK Low between Frames ; SCR = 1



With SCR= 1  your SPI clock is 48MHz / (2*2) = 12MHz  :)
0 件の賞賛
返信