LPC1114 GPIO voltage levels

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1114 GPIO voltage levels

1,969 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vladimirro on Sat Jun 20 13:07:18 MST 2015
Hello again

Let me introduce another problem I faced with LPC1114.
I tried to implement PWM and I noticed that the low state never reached 0V. It varied from 400mV to 600mV.

Then I set one of the GPIO to logic low and it turned out that my uC doesn't output 0V but 0,4-0,6V...
I couldn't find any information about voltage levels of GPIO in LPC1114 but I guess logic low should be 0V.
I probed the GND pin and it is 0V.

What can be a reason of such behaviour?
Labels (1)
0 Kudos
Reply
1 Reply

1,933 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sat Jun 20 15:20:35 MST 2015

Quote: vladimirro
I tried to implement PWM and I noticed that the low state never reached 0V. It varied from 400mV to 600mV.
...
What can be a reason of such behaviour?



Of course you should reach nearly 0V...

[img=660x397]http://www.lpcware.com/system/files/PWM_0.JPG[/img]

At least if your setup is correct, nothing is connected and your measurement equipment is working...
0 Kudos
Reply