LPC1114/444FBD48 IAP Code Size Issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1114/444FBD48 IAP Code Size Issue

1,715 次查看
john_zhou1
Contributor I

I am using NXP LPC1114/333 (56K flash) with keil 5.
Bootloader starts from 0 and App starts at 0x1000
App works fine when BIN size is 24,384 Bytes or smaller:
Program Size: Code=22604 RO-data=1452 RW-data=1020 ZI-data=1228

But not larger.
When I set App runs from 0, the flash size limit issue is gone, so codes were fine.

Where should I start to get rid of this?

Thank you!

ZQ

0 项奖励
回复
2 回复数

1,708 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suggest you generate a memory map file based on your application code with Keil and check if the code/constant data are saved in flash correctly, if there is issue, check if the linker file has issue.

BR

XiangJun Rong

标记 (1)
0 项奖励
回复

1,705 次查看
john_zhou1
Contributor I

Hello dear xiangjun_rong:

Thanks for the fast reply.

I have generated Maps for both working and not working BINs and did not have any clues.

I am located in Beijing, China. May I request an offline support or phone call? Because this is urgent, even paid tech support are acceptable. 

 

Thank you!

0 项奖励
回复