LPC1114/444FBD48 IAP Code Size Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1114/444FBD48 IAP Code Size Issue

1,673件の閲覧回数
john_zhou1
Contributor I

I am using NXP LPC1114/333 (56K flash) with keil 5.
Bootloader starts from 0 and App starts at 0x1000
App works fine when BIN size is 24,384 Bytes or smaller:
Program Size: Code=22604 RO-data=1452 RW-data=1020 ZI-data=1228

But not larger.
When I set App runs from 0, the flash size limit issue is gone, so codes were fine.

Where should I start to get rid of this?

Thank you!

ZQ

0 件の賞賛
返信
2 返答(返信)

1,666件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suggest you generate a memory map file based on your application code with Keil and check if the code/constant data are saved in flash correctly, if there is issue, check if the linker file has issue.

BR

XiangJun Rong

タグ(1)
0 件の賞賛
返信

1,663件の閲覧回数
john_zhou1
Contributor I

Hello dear xiangjun_rong:

Thanks for the fast reply.

I have generated Maps for both working and not working BINs and did not have any clues.

I am located in Beijing, China. May I request an offline support or phone call? Because this is urgent, even paid tech support are acceptable. 

 

Thank you!

0 件の賞賛
返信