LPC1112 programming problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1112 programming problem

1,108 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Sebastien Jacquemard on Thu Apr 25 23:34:04 MST 2013

Hello,


I've got problems to program LPC1112F/101 (HVQFN33 case) :


I made 2 verisons of PCB, first in January and second one in April.


I test the first one with success few month ago with LPC1112 revision "A" : (LPC1112F/101 - 918.105 - ZSD10300A)


The new board is also working with the same revision of the LPC1112.


Now old PCB and new PCB can't be prgorammed with new LPC1112 revision "B" (LPC1112F/101 - 536.118 - ZSD12211B).


I also try to connect a RS232 driver to drive RXD, TXD IAP and reset without success on the new board.


I use the last version of Keil (v4.70a), a J-Link Ultra from Segger with the last update. I've got message "Erase done" then "Flash timout".


I connect just the minimum PINS :


- Xtal (with a 12.0Mhz cristal)


- Vdd (pin6 and 9)


- Vss (with 100nF capacitors)


- IAP with 47K pullup to 3.3v


- Reset with 10K pullup and 100nF capacitor from ground


- To J-Link  : SWCLK, SWDIO, Ground, 3.3V and Reset


 


Any idea ?


 


Sebastien

标签 (1)
0 项奖励
回复
1 回复

1,087 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hkdnl on Wed May 01 03:26:51 MST 2013

Can you post the error message you get ?


 


And your schematic ?


0 项奖励
回复