LPC1100-based LPC-Link 2 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1100-based LPC-Link 2 ?

Jump to solution
2,550 Views
IvoBCD
Contributor III

We're considering using an LPC-Link 2 debugger (OM13054UL) to program devices.  Our distributors (eg. Element14) provide two variants of this debugger, one based on LPC1100, and another based on LPC4300.

OM13054UL-variants.png

On NXP's website, I can only find information about the LPC4300-based variant.

Is there really an LPC1100-based LPC-Link 2 ?  Can it be used instead of the LPC4300-based variant ?  If so, where can I find CMSIS-DAP firmware for the LPC1100-based LPC Link 2 ?

Best regards,

Ivo.

Labels (2)
Tags (1)
1 Solution
2,451 Views
converse
Senior Contributor V

NO, there is only one version of LPC-Link2 - it contains an LPC4300 device. It can, of course, be used to debug any NXP ARM Cortex-M based device.

View solution in original post

2 Replies
2,452 Views
converse
Senior Contributor V

NO, there is only one version of LPC-Link2 - it contains an LPC4300 device. It can, of course, be used to debug any NXP ARM Cortex-M based device.

2,451 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Ivo Clarysse,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
There's no such an LPC-link2 debug probe version that uses the LPC1100.
Hope this is clear.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------