LPC1000 line is death or obsolete?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1000 line is death or obsolete?

Jump to solution
2,262 Views
fjrg76
Contributor IV

I've noticed with sad that the newest MCUXpresso-IDE release doesn't include support for any microcontroller from the LPC1000 line

I have a custom board featuring the LPC1227FBD48  mcu that I need to program, but I didn't find any library support in the IDE.

 

LPC1000 is death?

Captura de pantalla de 2025-07-12 15-13-37.png

Labels (2)
0 Kudos
Reply
1 Solution
2,218 Views
fjrg76
Contributor IV

Yes, it's death ... Hello ST, it's me again!

Captura de pantalla de 2025-07-13 21-42-55.png

View solution in original post

0 Kudos
Reply
4 Replies
2,200 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @fjrg76 

Yes, LPC12xxx is legacy product, it is out of longevity.

We recommend the MCX series.

Product Longevity | NXP Semiconductors

Harry_Zhang_0-1752639426122.png

BR

Harry

0 Kudos
Reply
2,022 Views
danielholala
Senior Contributor II

@Harry_Zhang wrote:

We recommend the MCX series.

 

 

Why?

What about recent products from the LPC series, e.g., LPC552x or LPC553x?

 

0 Kudos
Reply
2,006 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @danielholala 

Because the MCX series are our new products.

Of course, you can choose LPC552x or LPC553x.

BR

Harry

0 Kudos
Reply
2,219 Views
fjrg76
Contributor IV

Yes, it's death ... Hello ST, it's me again!

Captura de pantalla de 2025-07-13 21-42-55.png

0 Kudos
Reply