LPC slave core reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC slave core reset

1,041 Views
ahmedsayed
Contributor I

Hello,

I'm using LPC54114 Dual core mcu I have imported dual core example (lpcxpresso54114_rpmsg_lite_pingpong_cm4) and it is working as expected but i need to add a bootloader to the example starting from adderss 0x0- 0x8000 the bootloader after finishing it's job it jumps to the application which has an offset 0x8000 but it seems the master core only works while the slave core stuck in the kMCMGR_ResetCoreState so did i miss some thing to add an offset 0x8000 to my application to have both cores working properly.

thanks in advance  

0 Kudos
Reply
1 Reply

994 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @ahmedsayed 

Based on your needs, i think  you can refer to the 

OTA Process introduction.

BR

Harry

0 Kudos
Reply