LPC-link 2 is stopped detected by system

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-link 2 is stopped detected by system

2,480 Views
priyadarshinisi
Contributor II

Hello,

I am using LPC-Link 2 for debugging my LPC1769 board. It was working fine till now, but suddenly it stopped working.

Here I meant by Stopped working is, now my LPC-link 2 is not detected by my system. I tried a different system, changing com ports and various cable too but still, LPC-link 2 device is not detected by any of the systems. LED1(bootLed) is blinking whenever I connect LPC-Link 2 with USBcable.

Anyone can help in finding what is basically the problem with my LPC-link 2 and how I can fix it.

lpcwarelpcware-supportlpcxpresso_support‌ 

#lpclink2#nxp lpc1769‌ 

Tags (2)
0 Kudos
Reply
5 Replies

2,246 Views
lpcxpresso_supp
NXP Employee
NXP Employee

So are you trying to use your LPC-Link2 with LPCXpresso IDE and letting LPCXpresso IDE softload the probe firmware? Or have you preprogrammed the Link2's flash with probe firmware using LPCScrypt?

https://community.nxp.com/message/630661 

And have you actually tried any of the troubleshooting suggestions at all in the FAQ we previously pointed you at?

Regards,

LPCXpresso Support

0 Kudos
Reply

2,246 Views
priyadarshinisi
Contributor II

I am using LPC-Link2 with LPCXpresso IDE and letting LPCXpresso IDE

softload the probe firmware.

A few days ago LPC Link-2 was performing well.

I was able to see "LPC Device" in my device and drivers.

Suddenly, Out of the box. It stopped detecting by my system (even I tried

other systems too.)

0 Kudos
Reply

2,246 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Check out : https://community.nxp.com/message/630577 

If you still have problems, give details of what you see in see at each stage of the manual boot process in Devices and Printers (assuming you are using Windows).

Regards,

LPCXpresso Support

0 Kudos
Reply

2,246 Views
priyadarshinisi
Contributor II

My LPC-Link 2 is not visible at  Devices and Printers.

0 Kudos
Reply

924 Views
ravicha
Contributor II

did u get the solution i face the same problem i am try to connect mcxc243 with link 2 before it connect but now it is not able to connect so please can u help me with your solution , Thanks

0 Kudos
Reply