LPC-link 2 is stopped detected by system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC-link 2 is stopped detected by system

2,472件の閲覧回数
priyadarshinisi
Contributor II

Hello,

I am using LPC-Link 2 for debugging my LPC1769 board. It was working fine till now, but suddenly it stopped working.

Here I meant by Stopped working is, now my LPC-link 2 is not detected by my system. I tried a different system, changing com ports and various cable too but still, LPC-link 2 device is not detected by any of the systems. LED1(bootLed) is blinking whenever I connect LPC-Link 2 with USBcable.

Anyone can help in finding what is basically the problem with my LPC-link 2 and how I can fix it.

lpcwarelpcware-supportlpcxpresso_support‌ 

#lpclink2#nxp lpc1769‌ 

タグ(2)
0 件の賞賛
返信
5 返答(返信)

2,238件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

So are you trying to use your LPC-Link2 with LPCXpresso IDE and letting LPCXpresso IDE softload the probe firmware? Or have you preprogrammed the Link2's flash with probe firmware using LPCScrypt?

https://community.nxp.com/message/630661 

And have you actually tried any of the troubleshooting suggestions at all in the FAQ we previously pointed you at?

Regards,

LPCXpresso Support

0 件の賞賛
返信

2,238件の閲覧回数
priyadarshinisi
Contributor II

I am using LPC-Link2 with LPCXpresso IDE and letting LPCXpresso IDE

softload the probe firmware.

A few days ago LPC Link-2 was performing well.

I was able to see "LPC Device" in my device and drivers.

Suddenly, Out of the box. It stopped detecting by my system (even I tried

other systems too.)

0 件の賞賛
返信

2,238件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Check out : https://community.nxp.com/message/630577 

If you still have problems, give details of what you see in see at each stage of the manual boot process in Devices and Printers (assuming you are using Windows).

Regards,

LPCXpresso Support

0 件の賞賛
返信

2,238件の閲覧回数
priyadarshinisi
Contributor II

My LPC-Link 2 is not visible at  Devices and Printers.

0 件の賞賛
返信

916件の閲覧回数
ravicha
Contributor II

did u get the solution i face the same problem i am try to connect mcxc243 with link 2 before it connect but now it is not able to connect so please can u help me with your solution , Thanks

0 件の賞賛
返信