LPC architecure good practices

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC architecure good practices

3,143 次查看
javiervallori
Contributor III

Hi,

I come from developing products with Microchip architecture. Now we start developing with LPC architecure, but I have some questions. In Microchip, before any read/write pin operation, it is highly recommended to "retris" the pin in INPUT/OUTPUT direction correspondingly. Is this "retris" operation also recommended for LPC? is there any other kind of good practice for LPC architecture?

0 项奖励
回复
5 回复数

2,896 次查看
soledad
NXP Employee
NXP Employee

Hi,

Maybe this link helps,

How to create a new LPC project using LPCOpen and LPCXpresso 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,896 次查看
okcn
Contributor III

What is "retris" ?

For LPC, before read/write Pin, should set INPUT/OUTPUT direction first.  this mode only need when sometime need input and sometime need output like data bus line.

If only need one operation in all time, set direction once is enough.

see manual and code samples for reference.

0 项奖励
回复

2,896 次查看
javiervallori
Contributor III

With "retris" I mean to set INPUT/OUTPUT direction before each INPUT/OUTPUT operation, even it is an always INPUT or an always OUTPUT pin. For example, Microchip recommends to set the direction every time you have to do a reading operation, because a noise can change accidentally this configuration. Is it this kind of operations also recommended in LPC architecture?

0 项奖励
回复

2,896 次查看
okcn
Contributor III

No.

In LPC, befor INPUT/OUTPUT operation, should set  INPUT/OUTPUT direction FIRST.

If always INPUT or  always OUTPUT, ONLY set direction ONCE is enough ! 

I did not experience any  noise for this. And no such info in manuals also. 

2,896 次查看
converse
Senior Contributor V

No, this is not necessary. NXP have not replicated Microchips bugs!