LPC USB device Detection to Host PC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC USB device Detection to Host PC

908 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by venkatesh on Thu Feb 14 02:31:21 MST 2013
Hi,

I am working on LPC1768 baord.
If i use mass storage firmware, this board is able to detect as LPC MASS STORAGE device in windows7/xp.

1. Now i am trying to make board as similar functions as custom device of USB class (client usb device) and should detect this board as their device in HOST(windows PC)..
So, Now i am able to map descriptor information in LPC as provided as custom USB device.(checked with USB analyzer tool).i hope during the enumeration time these will fetch by HOST and able to detect this LPC device as their Custom USB device. But its not happening.


Any one suggest me to check if i miss any thing to detect the device.

Thanks,
Venkatesh
Labels (1)
0 Kudos
Reply
0 Replies