LPC USB CDC Example Project Code Bugs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC USB CDC Example Project Code Bugs

1,191件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rlund on Thu Oct 16 12:40:42 MST 2014
I found two bug/issue/artifacts referenced in the USB CDC example project: usbd_rom_cdc_vcom.  One is "artf42016" and one is "artf45032".  The code related to these artifacts can by found in the project by searching the artifact numbers.  The workaround for these USB ROM "artifacts" is contained within the example project code, as opposed to fixing it at the source, in the library itself.  I have two questions:

Where/how can I find out more information about these two artifacts?

Are there other artifacts or bugs out there that I should be wary of with this code?

Any information or help on where to start answering these questions would be greatly appreciated.  Thanks!
ラベル(1)
0 件の賞賛
返信
0 返答(返信)