LPC Open for LPC2364

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC Open for LPC2364

2,237 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Nadasha on Tue Mar 17 23:23:48 MST 2015
Dear all,

           I am using LPCXpresso v7.6.2_326 IDE and LPC2364 controller. I tried to create an LPC open project for LPC2364,but  the option for creating LPC open project for LPC2x family was not present. Can someone please help me.


Regards,
Nadasha
标签 (1)
0 项奖励
回复
5 回复数

2,184 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Nadasha on Sat Mar 21 02:46:32 MST 2015
Thankyou.

But operating temperature and cost  are major problems. Operating temperature range should be suitable for automotive applications. i.e -40 to +125 oC. We are not able find an alternate controller meeting all our specs.


Regards,
Nadasha
0 项奖励
回复

2,184 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Mar 19 00:28:49 MST 2015
Example code for LPC2300 family is available from:

http://www.lpcware.com/node/11538/8,59

http://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc23xxlpc24xx-peripherals-using-keils-μvi...

But if you are just starting a new project, I would recommend that you consider using a newer Cortex-M based MCU rather than an old ARM7 based one though.

Regards,
LPCXpresso Support
0 项奖励
回复

2,184 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Nadasha on Wed Mar 18 22:51:11 MST 2015
I have to implement CAN,I2C, SPI,UART and SSI communication interface with the peripherals. So, is there any stack or library files available for LPC2364.
0 项奖励
回复

2,184 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Nadasha on Wed Mar 18 22:48:40 MST 2015
I have to implement CAN,I2C, SPI,UART and SSI communication interface with the peripherals. So, is there any stack or library files available for LPC2364.
0 项奖励
回复

2,184 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Mar 18 01:40:16 MST 2015
LPCOpen is only available for Cortex-M based microcontrollers, and not for the older ARM7 or ARM9 microcontrollers such as LPC2364.
0 项奖励
回复