LPC Open for LPC2364

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC Open for LPC2364

2,210件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Nadasha on Tue Mar 17 23:23:48 MST 2015
Dear all,

           I am using LPCXpresso v7.6.2_326 IDE and LPC2364 controller. I tried to create an LPC open project for LPC2364,but  the option for creating LPC open project for LPC2x family was not present. Can someone please help me.


Regards,
Nadasha
ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,157件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Nadasha on Sat Mar 21 02:46:32 MST 2015
Thankyou.

But operating temperature and cost  are major problems. Operating temperature range should be suitable for automotive applications. i.e -40 to +125 oC. We are not able find an alternate controller meeting all our specs.


Regards,
Nadasha
0 件の賞賛
返信

2,157件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Mar 19 00:28:49 MST 2015
Example code for LPC2300 family is available from:

http://www.lpcware.com/node/11538/8,59

http://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc23xxlpc24xx-peripherals-using-keils-μvi...

But if you are just starting a new project, I would recommend that you consider using a newer Cortex-M based MCU rather than an old ARM7 based one though.

Regards,
LPCXpresso Support
0 件の賞賛
返信

2,157件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Nadasha on Wed Mar 18 22:51:11 MST 2015
I have to implement CAN,I2C, SPI,UART and SSI communication interface with the peripherals. So, is there any stack or library files available for LPC2364.
0 件の賞賛
返信

2,157件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Nadasha on Wed Mar 18 22:48:40 MST 2015
I have to implement CAN,I2C, SPI,UART and SSI communication interface with the peripherals. So, is there any stack or library files available for LPC2364.
0 件の賞賛
返信

2,157件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Mar 18 01:40:16 MST 2015
LPCOpen is only available for Cortex-M based microcontrollers, and not for the older ARM7 or ARM9 microcontrollers such as LPC2364.
0 件の賞賛
返信