LPC_MRT->IRQ_FLAG address wrong

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC_MRT->IRQ_FLAG address wrong

896 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Wed Nov 05 05:41:40 MST 2014
Looking at the lpc8xx.h in CMSIS I found a problem.

The MRT definitions in the file contain:

typedef struct {
__IO uint32_t INTVAL; 
__IO uint32_t TIMER;         
__IO uint32_t CTRL;          
__IO uint32_t STAT;          
} MRT_Channel_cfg_Type;

typedef struct {
  MRT_Channel_cfg_Type Channel[4]; 
   uint32_t Reserved0[1]; 
  __IO uint32_t IDLE_CH; 
  __IO uint32_t IRQ_FLAG; 
} LPC_MRT_TypeDef;


but this places the IRQ_FLAG at address 0x4000  4048. The user manual mentions 0x4000 40f8
This means that the Reserved0[1] should be Reserved0[45] instead - and nog magically my code works  and that there is a bug in the NXP supplied lpc8xxx.h

Rob
Labels (1)
0 Kudos
Reply
1 Reply

885 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Wed Nov 05 07:05:30 MST 2014
Rob
Thank you for your feedback.
I believe you are correct.  I will report this to our software team.

Paul
0 Kudos
Reply