LPC-Linkv2 full speed usb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC-Linkv2 full speed usb

1,988件の閲覧回数
p_barcinski
Contributor I

I have an issue with programming via lpclinkv2 SWD interface on linux. LPC-Linkv2 doesn't accept full speed (12Mbps) usb and require high speed (480Mbps). I would like to use usb isolator which limits speed to full-speed but it doesn't work toogether. Is possible to force usb full-speed on lpclink and use this speed to flash/debug mcu?

0 件の賞賛
返信
1 返信

1,822件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello Piotr,

In order to better understand what you are trying to achieve. Could you please describe what your target mcu is as well?

So far my understanding is that you are connecting your LPC-Link 2 to your Linux machine on one end and then via SWD you are connecting your target mcu. However your LPC-link 2 is not communicating properly with your linux machine. Is this correct?

Could you please attach screen shots of any error messages that you are receiving.

Best Regards,

Sabina

0 件の賞賛
返信