LPC-Link2 with LPC55S0X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-Link2 with LPC55S0X

Jump to solution
2,160 Views
Jack_Star-int
Contributor I

I am working on a custom made board with LPC55S06/LPC5506 MCU. 

We have LPCXpresso55S06 EVK but we want to explore if LPC-LINK2(OM13054) could be able to work with MCUExpresso to debug and download firmware to the internal flash of our custom board. 

 

0 Kudos
Reply
1 Solution
2,147 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Jack_Star-int,

As it mention in the LPC-Link webpage, the LPC5000 family is supported. The webpage still doesn't add the LPC550x but is from the same family.

Best Regards,
Alexis Andalon

View solution in original post

0 Kudos
Reply
2 Replies
2,148 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Jack_Star-int,

As it mention in the LPC-Link webpage, the LPC5000 family is supported. The webpage still doesn't add the LPC550x but is from the same family.

Best Regards,
Alexis Andalon

0 Kudos
Reply
2,137 Views
Jack_Star-int
Contributor I

Hi @Alexis_A ,

Thanks for your explanation. I will get the LPC-Link and have it tested with my custom board.

Thanks,

Jack.L

0 Kudos
Reply