LPC-Link2 with LPC55S0X

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC-Link2 with LPC55S0X

跳至解决方案
2,299 次查看
Jack_Star-int
Contributor I

I am working on a custom made board with LPC55S06/LPC5506 MCU. 

We have LPCXpresso55S06 EVK but we want to explore if LPC-LINK2(OM13054) could be able to work with MCUExpresso to debug and download firmware to the internal flash of our custom board. 

 

0 项奖励
回复
1 解答
2,286 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Jack_Star-int,

As it mention in the LPC-Link webpage, the LPC5000 family is supported. The webpage still doesn't add the LPC550x but is from the same family.

Best Regards,
Alexis Andalon

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,286 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Jack_Star-int,

As it mention in the LPC-Link webpage, the LPC5000 family is supported. The webpage still doesn't add the LPC550x but is from the same family.

Best Regards,
Alexis Andalon

0 项奖励
回复
2,276 次查看
Jack_Star-int
Contributor I

Hi @Alexis_A ,

Thanks for your explanation. I will get the LPC-Link and have it tested with my custom board.

Thanks,

Jack.L

0 项奖励
回复