LPC-Link2 speed?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC-Link2 speed?

跳至解决方案
2,683 次查看
danielholala
Senior Contributor II

Hello,

I'd like to know the speed of the LPC-Link2 debug probe but could not find any information about it.

Especially, what is

  • download speed into RAM
  • max. target interface speed
  • max. SWO speed

Segger provides a nice chart providing this information for the J-Link probes here.

Gathering this information facilitates comparison of different probes.

Thanks.
Dan

0 项奖励
回复
1 解答
2,662 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

 

Hello danielholala, 

After confirm with internal, share the below information:

 

LPCLink2 use HS USB, and maximum SWD speed is about 4MHz

  • download speed into RAM: ~50KB/s
  • max. target interface speed: you mean SWD clock speed? ~4MHz.
  • SWO speed: ~4Mh

 

Hope it helps,

 

Alice

在原帖中查看解决方案

2 回复数
2,663 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

 

Hello danielholala, 

After confirm with internal, share the below information:

 

LPCLink2 use HS USB, and maximum SWD speed is about 4MHz

  • download speed into RAM: ~50KB/s
  • max. target interface speed: you mean SWD clock speed? ~4MHz.
  • SWO speed: ~4Mh

 

Hope it helps,

 

Alice

2,651 次查看
abnxpweb
Contributor III

Given that on many devices you can get flash programming speeds way in excess of the speed you quote for writing to RAM, I suspect your figures are somewhat out!

0 项奖励
回复