LPC-Link2 speed?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-Link2 speed?

Jump to solution
2,634 Views
danielholala
Senior Contributor II

Hello,

I'd like to know the speed of the LPC-Link2 debug probe but could not find any information about it.

Especially, what is

  • download speed into RAM
  • max. target interface speed
  • max. SWO speed

Segger provides a nice chart providing this information for the J-Link probes here.

Gathering this information facilitates comparison of different probes.

Thanks.
Dan

0 Kudos
Reply
1 Solution
2,613 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

 

Hello danielholala, 

After confirm with internal, share the below information:

 

LPCLink2 use HS USB, and maximum SWD speed is about 4MHz

  • download speed into RAM: ~50KB/s
  • max. target interface speed: you mean SWD clock speed? ~4MHz.
  • SWO speed: ~4Mh

 

Hope it helps,

 

Alice

View solution in original post

2 Replies
2,614 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

 

Hello danielholala, 

After confirm with internal, share the below information:

 

LPCLink2 use HS USB, and maximum SWD speed is about 4MHz

  • download speed into RAM: ~50KB/s
  • max. target interface speed: you mean SWD clock speed? ~4MHz.
  • SWO speed: ~4Mh

 

Hope it helps,

 

Alice

2,602 Views
abnxpweb
Contributor III

Given that on many devices you can get flash programming speeds way in excess of the speed you quote for writing to RAM, I suspect your figures are somewhat out!

0 Kudos
Reply