LPC Link2 debug i.MX RT1052 EVKB failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC Link2 debug i.MX RT1052 EVKB failed

ソリューションへジャンプ
3,057件の閲覧回数
lognight
Contributor III

Hi NXP,

I bought a LPC Link2 hardware and used it to debug i.MX RT1052 EVKB board, but I met some issues.

Before start debug, the LPC LInk2 can be found. see below pic

1.PNG

and next steps, download image, and stop in main function, are all OK. but when I click go button, after a while, there is an error, see below pic

3.PNG

then I have no any chance to debug rt1052 evkb board, even I terminal this debug session and restart.

below pic is debug console infomations when I debug rt1052 evkb board.

4.PNG

when I restart debug, the LPC Link2 DAP cannot be found.

I tried many times, no one time I successed. 

other infomation:

I connect LPC Link2 board  J7 port  to i.MX RT1052 evkb board JTAG port using an adapt board, below is the adapt board schematic and my hardware connection.

147007505.jpg

761058129.jpg

the MCUXpresso IDE version I used is V11.1.0.

 

What's wrong with this?  Is my LPC Link2 board broken? 

ラベル(2)
0 件の賞賛
返信
1 解決策
2,974件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi steven zhang,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I find that the JP1 is open, it means that it won't load the firmware which resides in the QSPI flash, please close the JP1 with a jumper and give a try again.

pastedImage_1.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,974件の閲覧回数
lognight
Contributor III

It's solved. Thanks for your reminding.

0 件の賞賛
返信
2,975件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi steven zhang,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I find that the JP1 is open, it means that it won't load the firmware which resides in the QSPI flash, please close the JP1 with a jumper and give a try again.

pastedImage_1.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------