LPC Link2 and EmWin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC Link2 and EmWin

1,002件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TBaxter on Fri Apr 11 12:04:25 MST 2014
I’m using EmWin – I’m working with the graph function – I have created objects and a couple of markers that I move back and forth along the graph. The problem I’m having is that the graph appears to redrawing all the objects when I move a marker along the graph and it slows up the functionality the more objects I have on the graph. Is there away (or any sample code) that would allow me just to redraw the marker and not the whole object. I'm thinking I need to use the validate call but there done not seem to be one for the graph object – anyway and help on this would be appreciated. Thanks!
ラベル(1)
0 件の賞賛
返信
0 返答(返信)