LPC Link2 Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC Link2 Error

7,065 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by grillkopf on Sun Jun 08 08:57:49 MST 2014
Hi.
I've bought a LPC Link2 and tried to program my LPC1788. But LPCXpresso throws some errors.

#1
Error in final launch sequence
Failed to execute MI command:
-target-select extended-remote | crt_emu_cm_redlink -msg-port=1740 -g -mi -2 -pLPC1788 -vendor=NXP -reset= -ProbeHandle=1 -CoreIndex=0 -flash-driver=LPC177x_8x_407x_8x_512.cfx
Error message from debugger back end:
Remote communication error.  Target disconnected.: No error.
Remote communication error.  Target disconnected.: No error.

#2
02: Failed on connect
  02: Failed on connect
  Could not connect to core.
  31: No connection to emulator device

I tried it for several hours. I definetly won't recommend LPCxxxx Devices and LPCXpresso. There are unfortunately too many problems. :(

Can anyone tell me a sulution for my problem. I googled the errors but nothing worked.
Thanks

Labels (1)
0 Kudos
Reply
17 Replies

6,930 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by grillkopf on Thu Jul 24 12:20:56 MST 2014
Update:

I found out, that LPCXpresso is supporting J-Link. I have an Jlink EDU and it worked. I made an new project, added CMSIS and the other libraries and did a few integer operations. It worked well. But why does the LPC Link2 not work??
0 Kudos
Reply

6,930 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by grillkopf on Thu Jul 24 11:35:53 MST 2014
Hello. I still wasn't able to fix the Problem. Does anyone know a solution. When I try to Debug a project, the debugger throws errors and I'm not able to connect to the core anymore.


with all the trouble I had, I won't buy any NXP product in  the future. I bought the board nearly 1 year ago and I'm not able to get it working :(.
0 Kudos
Reply

6,930 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by grillkopf on Mon Jun 09 14:19:01 MST 2014
Hello.
thanks for the help... I'm sure I made a mistake in my Project. I will try the demo projects.

Tank you
0 Kudos
Reply

6,930 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Jun 09 00:59:24 MST 2014
I would also strongly recommend that you carefully read the user manual for your board, available directly from the Embedded Artists website.

http://www.embeddedartists.com/products/kits/lpc1788_kit.php

These boards have a large number of jumpers, and if these are not correctly set, then you may experience issues with debugging.


Regards,
LPCXpresso Support

0 Kudos
Reply

6,930 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sun Jun 08 13:35:07 MST 2014
This Video is showing how to connect LPC-Link2 and switch to ISP...

http://www.youtube.com/watch?v=ZBruOIbSTME
0 Kudos
Reply

6,930 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Sun Jun 08 11:29:14 MST 2014
Resetting the board into ISP mode is guaranteed to recover, unless you have used one of the higher CRP modes. Therfore, I suspect that you didn't follow the ISP resetting instructions properly. Either that, or your board is damaged (which is unlikely).
0 Kudos
Reply

6,930 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by grillkopf on Sun Jun 08 11:15:58 MST 2014
The Board is powered externally, with my Power supply over the 5V jack. Powersupply can drive the Board easily (max current 40A)
0 Kudos
Reply

6,930 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Sun Jun 08 11:02:43 MST 2014
Also, how are you powering the ea board?
0 Kudos
Reply

6,930 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sun Jun 08 10:48:02 MST 2014

Quote: grillkopf
I connected the LPC Link 2 to J7 on the Board.



:quest:

Link2-J7 has to be connected to EA-Kit-J7. Red stripe of ribbon cable shows pin1 of EA-Kit-J7.

Whatever you have flashed, switching to ISP should regain access to MCU again because it's using default clock settings (IRC). If you delete MCU with FlashMagic it's also in ISP mode (because it's blank) and SWD should work... 

0 Kudos
Reply

6,930 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by grillkopf on Sun Jun 08 10:28:28 MST 2014

I connected the LPC Link2 to my PC and with that small cable (i don't know the english name for that grey cable with 10 pins. I'm German) I connected the LPC Link 2 to J7 on the Board. I think my flashed program  destroyed the connection, but I included the CMSIS libs. The code for initializing pll etc is also there, so i dont know why my application destroyed the SWD function...


0 Kudos
Reply

6,930 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sun Jun 08 10:22:51 MST 2014
LPC-Link2 and 'LPC1788 Developer’s Kit' is working without problems here.

How did you connect it?

0 Kudos
Reply

6,930 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by grillkopf on Sun Jun 08 10:15:23 MST 2014
But Flash Magic is really slow. It needs almost 5 minutes to flash the demo...

Is there any way to programm using the LPC Link2?
0 Kudos
Reply

6,930 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sun Jun 08 10:12:17 MST 2014

Quote: grillkopf
But how's it even possible that you loose control of the debug function?



There a several options to destroy SWD functions. Wrong clock setup, pin settings....


Quote: grillkopf
That didn't work.



If SWD isn't working after switching to ISP you have to use FlashMagic and UART Bootloader as described in 'LPC1788 Developer’s Kit User’s Guide'...
0 Kudos
Reply

6,930 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by grillkopf on Sun Jun 08 10:05:05 MST 2014
Sorry.
But how's it even possible that you loose control of the debug function?



Quote:
So just switch to ISP: Push SW6 (ISP button) and reset the board via SW1 (Reset button).

Then try to flash/debug it again...



That didn't work.
0 Kudos
Reply

6,930 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sun Jun 08 09:30:46 MST 2014
See: http://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access

UM:
4.12 SP8: Digital IO
There is a push-button (SW6) that is connected to a signal that enable the ISP-mode after reset on the
OEM Board. For the LPC1788 this is pin P2.10.

So just switch to ISP: Push SW6 (ISP button) and reset the board via SW1 (Reset button).

Then try to flash/debug it again...

BTW: Are you sure you flashed a valid image?
0 Kudos
Reply

6,930 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by grillkopf on Sun Jun 08 09:15:01 MST 2014
its a Board from embedded Artists. The LPC1788 Board. I connected the LPC Link2 with the Board. the Board has Power and I was able to program the Board 1 time...

But now....
I've got no clue what's wrong
0 Kudos
Reply

6,930 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Sun Jun 08 09:08:24 MST 2014
Is it a custom board? Sounds like you have not wired up the debug connector correctly, or you are not supplying power to your chip. The clue is in th error message. Cannot connect to core - it means what it says.
0 Kudos
Reply