LPC Link2 Boar ADCHS input connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC Link2 Boar ADCHS input connection

945 次查看
cpchen
Contributor III

Hi, I like to test LPC4370 ADCHS capability , first I need to apply an analog input signal to LPC-link2 board, then I will practice with LPC4370 configuration and coding to test the ADCHS functionality.  I look the LPC-link 2 schematics and other document, but I am not sure where is the input pin for ADCHS。  

From Schematics , I see ADC input on J4 , asshown below.  

pastedImage_1.png

but I do not see the corresponding I/O on LPC4370 I/O, also on Schematics.   

pastedImage_2.png

Can someone tell me, 

1. Whether I can apply a signal in LPC link2 ,and gets to the LPC4370 ADCHS input ?

2. If I can, where and how ? 

Best Regards,

标记 (2)
0 项奖励
回复
0 回复数