LPC-Link-2 supportability for ETM in Keil

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC-Link-2 supportability for ETM in Keil

2,684件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ramana on Wed Jun 11 23:19:50 MST 2014
I am using LPC-Link-2 with Segger's J-link image. It is working great. Has many advantages when compared to other debuggers. But ETM is not detecting in Keil(uV4/uV5). But LPC-Link-2 is ETM fitted. Please help me to use this feature. Please verify attached image for error in Keil. I have also attached LPC-Link2 J-link image info. I have connected CPU to 20pin trace port of LPC-Link2.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,615件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Jun 12 00:32:29 MST 2014
The J-Link firmware provided by Segger for LPC-Link2 is basically J-Link Lite, which I believe does not support ETM trace.

http://www.segger.com/lpc-link-2.html

Regards,

LPCXpresso Support
0 件の賞賛
返信

2,615件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Thu Jun 12 00:32:21 MST 2014
Given the restrictions that Segger have placed on this image, I would guess that ETM is not supported:

[list]
  [*]   The firmware is only to be used with NXP target devices. Using it with other devices is prohibited and illegal.
  [*]    The firmware is for use with evaluation boards only. It is not for use with custom hardware.
  [*]    The firmware may only be used for development and/or evaluation purposes. It may not be used for production purposes.
  [*]    The firmware is made available without any warranty and without support.
[/list]
http://www.segger.com/lpc-link-2.html
0 件の賞賛
返信