LPC-LINK2 OPENOCD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-LINK2 OPENOCD

4,207 Views
yuanbinzhou
Contributor II

Hi all,

I am trying to use LPC-LINK2 and openocd under ubuntu 16.04 recently. LPC-Link2 has been programed with JLINK firmware.

openocd:Open On-Chip Debugger 0.9.0 

board:lpc1837

I used the command to connect with the board: openocd -f interface/jlink.cfg -f board/lpc1850_spifi_generic.cfg

However it got the following errors:

adapter speed: 500 kHz
cortex_m reset_config sysresetreq
Info : J-Link LPC-Link 2 compiled May 30 2016 16:15:37
Info : J-Link caps 0xb9ff7bbf
Info : J-Link hw version 18010000
Info : J-Link hw type J-Link on LPC-Link2
Info : J-Link max mem block 35912
Info : J-Link configuration
Info : USB-Address: 0xff
Info : Kickstart power on JTAG-pin 19: 0xffffffff
Info : Vref = 3.300 TCK = 1 TDI = 0 TDO = 1 TMS = 0 SRST = 1 TRST = 1
Info : J-Link JTAG Interface ready
Info : clock speed 500 kHz
Error: JTAG scan chain interrogation failed: all ones
Error: Check JTAG interface, timings, target power, etc.
Error: Trying to use configured scan chain anyway...
Error: lpc1850.m3: IR capture error; saw 0x0f not 0x01
Warn : Bypassing JTAG setup events due to errors
Warn : Invalid ACK 0x7 in JTAG-DP transaction
Warn : Invalid ACK 0x7 in JTAG-DP transaction
Warn : Invalid ACK 0x7 in JTAG-DP transaction
Warn : Invalid ACK 0x7 in JTAG-DP transaction
Warn : Invalid ACK 0x7 in JTAG-DP transaction
Warn : Invalid ACK 0x7 in JTAG-DP transaction
Warn : Invalid ACK 0x7 in JTAG-DP transaction
Warn : Invalid ACK 0x7 in JTAG-DP transaction
Warn : Invalid ACK 0x7 in JTAG-DP transaction
Warn : Invalid ACK 0x7 in JTAG-DP transaction

It seems that there is no any differences with lpc1850 and lpc1837 in configuration file.What is wrong with it? What should I do next?

Labels (2)
0 Kudos
Reply
1 Reply

2,722 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Yuanbin Zhou,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

To provide the fastest possible support I want to point you to a 
similar question which has been answered on our NXP community. 
to view the details.

Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply