LPC-LINK2 BOARD DEBUG ERROR?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-LINK2 BOARD DEBUG ERROR?

1,904 Views
aravindpb5009
Contributor III

HAI 

           I tried to debug the code through the lpc-link 2 board (OM13054) but finally i got some appearance  on mcuxpresso ide   my controller (LPC824)  in below image showed what error shown in my project plz let me know the solution for the error

Thanks & Regards

Aravind P

Labels (7)
0 Kudos
Reply
1 Reply

1,804 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Aravind palanisamy,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Whether you program and debug the LPC824 board successful before, to locate the issue, I'd like to suggest you follow the method to confirm the debug interface is correct.
1. Update the LPC-link2 with the J-link firmware.
2. Connect the LPC-link2 to the LPC824 board.
3. Open the J-Link Commander to check whether the core is able to be recognized.
If the core has been recognized, it means that the hardware circuit is correct, you can delete the project in the MCUXpresso IDE and reimport it again, then give debug a try.


Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply