LPC LINK2 AND LPC1115

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC LINK2 AND LPC1115

1,189 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by otxoasound on Sun May 04 13:41:05 MST 2014
Hello
            I tried to find the way to connect lpclink2 and lpcxpresso 1115 eval board, but I could not find information about how to do it. I know I have to cut the traces (J4 connector on LPC1115). Lpclink2 J6 connector has 9 pin and lpcxrpesso 1115 eval board J4 has 8 pin, so how I connect them?  I want to use lpclink2 as debug tool with lpcxpresso 1115 eval board.  Somebody ask a similar question in this forum, but I can not see how the connection is made, because the picture which sent the support people is ambiguous. Somebody could help me?

                               Thank you in advance.
Labels (1)
0 Kudos
Reply
1 Reply

1,174 Views
lpcware
NXP Employee
NXP Employee
0 Kudos
Reply