LPC 802 & LPC 804 Microcontroller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC 802 & LPC 804 Microcontroller

跳至解决方案
1,603 次查看
VIGNESH_BABU
Contributor II

Hi;

I am using the LPC 802 and LPC804 Microcontroller with 15MHz of Frequency. I wants to toggle the pin for every 400ns.

Where I can able to toggle the pin using timer only up to 10 microsecond and in polling method can able to toggle upto 3-5 microsecond(nearly 300 KHz) only. Please suggest the Idea to generate the Clock up to 2.4 MHz or toggle of LED for every 400 ns in the LPC802 and LPC804 Microcontroller.

Thank you

0 项奖励
回复
1 解答
1,597 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that you use CTimer to generate interrupt with a fixed period, in the ISR, you clear the CTimer status bit and toggle a LED. Because the interrupt handling requires a lot of time, for example pushing core registers to stack, pop the core registers from stack, jumping ISR, so the ISR frequency is low.

I suggest you use CTimer to generate PWM signal to drive LED, I am sure that the PWM frequency can reach up to 2.4mhz, pls check if the solution can meet your requirement.

BR

XiangJun Rong

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,598 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that you use CTimer to generate interrupt with a fixed period, in the ISR, you clear the CTimer status bit and toggle a LED. Because the interrupt handling requires a lot of time, for example pushing core registers to stack, pop the core registers from stack, jumping ISR, so the ISR frequency is low.

I suggest you use CTimer to generate PWM signal to drive LED, I am sure that the PWM frequency can reach up to 2.4mhz, pls check if the solution can meet your requirement.

BR

XiangJun Rong

 

0 项奖励
回复