LPC 802 & LPC 804 Microcontroller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC 802 & LPC 804 Microcontroller

Jump to solution
1,523 Views
VIGNESH_BABU
Contributor II

Hi;

I am using the LPC 802 and LPC804 Microcontroller with 15MHz of Frequency. I wants to toggle the pin for every 400ns.

Where I can able to toggle the pin using timer only up to 10 microsecond and in polling method can able to toggle upto 3-5 microsecond(nearly 300 KHz) only. Please suggest the Idea to generate the Clock up to 2.4 MHz or toggle of LED for every 400 ns in the LPC802 and LPC804 Microcontroller.

Thank you

0 Kudos
Reply
1 Solution
1,517 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that you use CTimer to generate interrupt with a fixed period, in the ISR, you clear the CTimer status bit and toggle a LED. Because the interrupt handling requires a lot of time, for example pushing core registers to stack, pop the core registers from stack, jumping ISR, so the ISR frequency is low.

I suggest you use CTimer to generate PWM signal to drive LED, I am sure that the PWM frequency can reach up to 2.4mhz, pls check if the solution can meet your requirement.

BR

XiangJun Rong

 

View solution in original post

0 Kudos
Reply
1 Reply
1,518 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that you use CTimer to generate interrupt with a fixed period, in the ISR, you clear the CTimer status bit and toggle a LED. Because the interrupt handling requires a lot of time, for example pushing core registers to stack, pop the core registers from stack, jumping ISR, so the ISR frequency is low.

I suggest you use CTimer to generate PWM signal to drive LED, I am sure that the PWM frequency can reach up to 2.4mhz, pls check if the solution can meet your requirement.

BR

XiangJun Rong

 

0 Kudos
Reply