LPC 55S28 evk cmsis driver developement i2c

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC 55S28 evk cmsis driver developement i2c

1,393件の閲覧回数
vi77
Contributor I

Hi,

    I am new to lpc , working on lpc55s28 evaluation board, need to develop i2c drivers for it using cmsis in keil. I do not want to use the fsl drivers available , i went through the example projects provided using cmsis i2c it  uses the fsl i2c driver .However my aim is not to use the fsl drivers and develop a generic driver i2c  but i am not able to proceed ,can anybody suggest any documentation to start with or examples ,guide to write a i2c driver. Thanks

0 件の賞賛
返信
1 返信

1,388件の閲覧回数
KalaimaniArumugamdev
Contributor III

Hi,

 General sequence for design any peripheral without FSL file in nxp,

  •   Enable the peripheral and pot clock
  •   Enable port pin and update alternative function as I2C.
  •  All other peripheral configuration and control register update code available in user manual page 561 &562