LPC 546 USART CONFIG USING REGISTER

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC 546 USART CONFIG USING REGISTER

5,651 次查看
k_sunilgupta
Contributor II

Hi all,

 

i want to do register level programing using LPC546 to interface usart, anyone could help me.

This is my configuration for usart0 in LPC546 for polling mode:-

USART0->CFG |= (1UL << 0); // USART ENABLE
USART0->BRG = 115200U; // SET BAUDRATE
USART0->CFG = 0x0U; // NO PARITY
USART0->CFG &=~ (1UL << 6); // 1 STOP BIT
USART0->CFG = 0x1U; // 8 BIT DATA LENGTH

USART0->CFG &=~ (1UL << 11); // ASYNC MODE
USART0->CFG &=~ (1UL << 12); // FALLING EDGE*/

 

But its not working, please suggest id anyone known this thing.

 

 

 

0 项奖励
回复
13 回复数

5,640 次查看
k_sunilgupta
Contributor II

i have checked all bits but not finding error from my side, 

0 项奖励
回复

5,635 次查看
frank_m
Senior Contributor III

Did you think of enabling power and clock for the USART peripheral block ?

5,600 次查看
k_sunilgupta
Contributor II

I have POWER ON 

 

SYSCON->PDRUNCFG[0] |= (1 << 4)

AND I did not find clock for USART pheripheral block in user mannual, Please help me to creak this

0 项奖励
回复

5,581 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

If your USART is from FlexComm0, you need to make sure there is clock attaching to FlexComm0.

Please check USART demo code, CLOCK_AttachClk

0 项奖励
回复

5,578 次查看
k_sunilgupta
Contributor II

SYSCON->AHBCLKCTRL[1] |= (1UL << 11); // FLEXCOMM0 CLOCK ENABLE
SYSCON->FCLKSEL[0] = 0x4U;
SYSCON->FRGCTRL = 0x01;

void USART_0_INIT(void)
{

USART0->CFG |= (1 << 0); // USART ENABLE
USART0->BRG = 0x67; // SET BAUD RATE
USART0->CFG &=~ (1 << 6); // 1 STOP BIT
USART0->CFG |= (1 << 2); // 8 BIT MODE
USART0->FIFOCFG |= (1 << 16) | (1 << 0); // ENABLE TX
USART0->FIFOCFG |= (1 << 17) | (1 << 1); // ENABLE RX
USART0->CFG &=~ (1 << 11); // ASYNC MODE
USART0->CFG &=~ (1 << 12); // FALLING EDGE

}

0 项奖励
回复

5,577 次查看
k_sunilgupta
Contributor II

please check the code i have done the needful

0 项奖励
回复

5,573 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

 

Suggest you testing usart_polling SDK demo as a standard on the board. thus we can know if HW environment is ok.

If demo code works but your code can't,  make register comparison of demo and your code in debug code.

 

0 项奖励
回复

5,555 次查看
k_sunilgupta
Contributor II

have you ever config USART on register level programing ?

 

@ZhangJennie 

0 项奖励
回复

5,535 次查看
k_sunilgupta
Contributor II

please reply.

0 项奖励
回复

5,498 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

LPC546 only has SDK demo as official demo code. and I didn't test on other code.

If you don't use SDK, please follow the advice above, referring SDK usart demo, follow the usart initialization sequence and check the related register setting to config yours code.

0 项奖励
回复

5,549 次查看
frank_m
Senior Contributor III

> have you ever config USART on register level programing ?

Easy solution.

Take the proposed SDK USART example, determine the sequence of initialisation steps either via static code analysis or debugging, and apply it to your code.

0 项奖励
回复

5,486 次查看
k_sunilgupta
Contributor II

i have done it now its working fine on register level.

0 项奖励
回复

5,645 次查看
frank_m
Senior Contributor III

> i want to do register level programing using LPC546 to interface usart, anyone could help me.

Which is fine. But don't use magic numbers.

This forces others to read your code and the MCU manual in parallel, and crosscheck all your registers, bits, and shifts.

Many posters her like me are volunteers, and neither have the time nor the desire to do that.

Instead use the defines that come with the MCU-specific header in the SDK. For example, in LPC54628.h. That makes reading much easier.

0 项奖励
回复