LPC 43S67 and GainSpan GS2100M sdio adapter board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC 43S67 and GainSpan GS2100M sdio adapter board

1,880 Views
omidathari
Contributor II

Hello

I've got your LPCXpresso43xx/18xx with OM13082 and a GainSpan SDIO Wifi Adapter Board GS2100M.

I get an error when I run the example app from lpc_open "periph_sdio"

DBG: SDIO Card init error: 0xFFFFFFFE, -2

Any help is appreciated

Omid 

Labels (2)
0 Kudos
Reply
2 Replies

1,634 Views
omidathari
Contributor II

The sd/mmc socket on the OM13082 is not connected to vcc.

0 Kudos
Reply

1,634 Views
soledad
NXP Employee
NXP Employee

Hello Omid,

On the LPC4337 Xpresso shield board JP3 must be soldered to shunt, could you please double check this configuration?


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply