LPC 4350 SGPIO Camera interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC 4350 SGPIO Camera interface

1,332 次查看
dudisasson
Contributor I

Hi,

i am trying to use the LPC4350 SGPIO camera interface. 

i followed the example code and i am able to get the data the camera. 

the problem is that until i get the data from the last slices, the content of the reg_ss is already changed.

the BASE_CLK_PERIPH is 200MB, the PIXCLK from the sensor is 20MB.

i am using the SGPIO interrupt from M4 and the SDRAM i am writing to is connected using the EMC interface.

the code i am using when getting an interrupt from slice A is as follows:

if (r->status_1 & 1)

{

r->clr_status_1 = 0x1;

{

*pxl_p++ = r->reg_ss[pin7Slice];

*pxl_p++ = r->reg_ss[pin6Slice];

*pxl_p++ = r->reg_ss[pin5Slice];

*pxl_p++ = r->reg_ss[pin4Slice];

*pxl_p++ = r->reg_ss[pin3Slice];

*pxl_p++ = r->reg_ss[pin2Slice];

*pxl_p++ = r->reg_ss[pin1Slice];

*pxl_p++ = r->reg_ss[pin0Slice];

}

any idea how can solve it?

Thanks,

Dudi.

0 项奖励
回复
1 回复

1,196 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Dudi,

Do you have tried to slow down the PIXCLK to 12MHz?

If the issue still there?


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复