LPC 4337 and 128Mb SDRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC 4337 and 128Mb SDRAM

跳至解决方案
1,784 次查看
michaeldenney
Contributor II

I am using the LPC4337 LQFP144  connecting to IS42S16800F-7  8Mx16 SDRAM chip.

I think I am setting up the EMC properly but I am not getting the results that I would expect.  Can anyone look at my setup and verify that I am not missing something.

void SDRAM_Init(void)
{
uint32_t pclk;
uint32_t temp;
uint64_t tmpclk;
uint32_t tmp2;

// divide core clock by 2 to get approx 102 Mhz
LPC_CREG->CREG6 |= (1 << 16);
LPC_CCU1->CLKCCU[CLK_MX_EMC_DIV].CFG |= (1 << 5);
//LPC_SCU->EMCDELAYCLK = 0x00006666;
pclk = Chip_Clock_GetEMCRate(); 

LPC_EMC->STATICWAITRD0 = NS2CLK(pclk,55); // select the delay from chip select 0 to a read access
LPC_EMC->STATICCONFIG0 = 0x81; // select memory config for static chip select 0
LPC_EMC->STATICWAITOEN0 = NS2CLK(pclk,10); // selects the delay from chip select 0 or address change to output enable
LPC_EMC->STATICWAITWEN0 = NS2CLK(pclk, 10); // selects the delay from chip select 0 to write enable
LPC_EMC->STATICWAITPAG0 = NS2CLK(pclk, 55); // selects the delay for async page mote access
LPC_EMC->STATICWAITWR0 = NS2CLK(pclk, 55); // selects the delay from chip select 0 to a write access
LPC_EMC->STATICWAITTURN0 = NS2CLK(pclk, 55); // selects the number of bus turnaround cycles for chip select 0

LPC_SCU->SFSCLK[0] = (MD_PLN_FAST | SCU_MODE_FUNC5);
LPC_SCU->SFSCLK[1] = MD_PLN_FAST;
LPC_SCU->SFSCLK[2] = (MD_PLN_FAST | SCU_MODE_FUNC5);
LPC_SCU->SFSCLK[3] = MD_PLN_FAST;

LPC_EMC->CONTROL = 0x00000001;
LPC_EMC->CONFIG = 0x00000000;
LPC_EMC->DYNAMICCONFIG0 =  (1 << 10) | (1 << 7);

LPC_EMC->DYNAMICRASCAS0 = 0x00000303;
LPC_EMC->DYNAMICREADCONFIG = 0x00000003;

LPC_EMC->DYNAMICRP = NS2CLK(pclk,20);
LPC_EMC->DYNAMICRAS = NS2CLK(pclk,42);
LPC_EMC->DYNAMICSREX = NS2CLK(pclk,63);

LPC_EMC->DYNAMICAPR = 0x00000005;
LPC_EMC->DYNAMICDAL = 0x00000005;
LPC_EMC->DYNAMICWR = 2;
LPC_EMC->DYNAMICRC = NS2CLK(pclk, 63);
LPC_EMC->DYNAMICRFC = NS2CLK(pclk, 63);
LPC_EMC->DYNAMICXSR = NS2CLK(pclk, 63);
LPC_EMC->DYNAMICRRD = NS2CLK(pclk, 14);
LPC_EMC->DYNAMICMRD = 0x00000002;

//Delay_us(100);
Delay_ms(100);
LPC_EMC->DYNAMICCONTROL = 0x00000183; /* Issue NOP command */

//Delay_us(200); /* wait 200ms */
Delay_ms(200);
LPC_EMC->DYNAMICCONTROL = 0x00000103; /* Issue PALL command */

LPC_EMC->DYNAMICREFRESH = EMC_SDRAM_REFRESH(pclk, 70); /* ( n * 16 ) -> 32 clock cycles */

//for(i = 0; i < 0x80; i++); /* wait 128 AHB clock cycles */
Delay_ms(200); /* wait 200ms */
tmpclk = (uint64_t) 15625 * (uint64_t) pclk / 1000000000 / 16;
LPC_EMC->DYNAMICREFRESH = tmpclk; /* ( n * 16 ) -> 736 clock cycles -> 15.330uS at 48MHz <= 15.625uS ( 64ms / 4096 row ) */

LPC_EMC->DYNAMICCONTROL = 0x00000083; /* Issue MODE command */

temp = *((volatile uint32_t *) (SDRAM_ADDR_BASE | (3 << 4 | 3 ) << 12)); /* 8 burst, 3 CAS latency */

temp = temp;
LPC_EMC->DYNAMICCONTROL = 0x00000000; /* Issue NORMAL command */

//[re]enable buffers
LPC_EMC->DYNAMICCONFIG0 = (1 << 19) | (1 << 10) | (1 << 7);

}

Test function

uint16_t data = 0x0102;
uint16_t rdData;

uint16_t *short_wr_ptr;
short_wr_ptr = (uint16_t *) SDRAM_ADDR_BASE;
uint16_t *short_rd_ptr;


short_rd_ptr = (uint16_t *) SDRAM_ADDR_BASE;

for (i=0; i<(0x01000000/2); i++)
{
   *short_wr_ptr++ = data;
   data += 0x0101;   

   rdData = *short_rd_ptr;
   if(rdData != 0x0102)
   {
      errorCount = i;

   }

}

The data seems to be getting corrupted early and and randomly.  By that I mean that within the first 14-400 writes my first address has been overwritten and it does not seem to correspond to any specific address line.

Any help would be greatly appreciated.

Thank you

Michael Denney

标签 (2)
标记 (2)
0 项奖励
回复
1 解答
1,329 次查看
michaeldenney
Contributor II

For those who may care,

The problems I had were related to interrupts (as is usually the case). I had a function in an interrupt that was reading and writing values to the flash.  Therefore my data was getting corrupted during my testing.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,330 次查看
michaeldenney
Contributor II

For those who may care,

The problems I had were related to interrupts (as is usually the case). I had a function in an interrupt that was reading and writing values to the flash.  Therefore my data was getting corrupted during my testing.

0 项奖励
回复
1,329 次查看
michaeldenney
Contributor II

Update...

If I step through the code one write and one read at a time the data appears to be good.  If I let the program run at all then the data gets corrupted.

If I add a delay between the write and the read the data gets corrupted.

does this have something to do with the refresh rate?

anyone else have an issue like this?  

0 项奖励
回复