LPC 24xx ISP locked

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC 24xx ISP locked

1,400件の閲覧回数
michalmatejka
Contributor I

We have LPC 2468 with internal flash and need to reprogramme with our code by ISP. Probleme is, that IC is locked and setted security...Is a way to un-lock device, erase  and burn new code. We use Flash Magic ..

ラベル(2)
0 件の賞賛
返信
1 返信

1,235件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Michal,

You mean the CRP has been implemented? if CRP1/2 is set, you can use FlashMagic to erase the flash.

If CRP3 is set, ISP mode only can be entered by user code.

161426_161426.pngpastedImage_1.png

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信