LPC 2138 unable to read from flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC 2138 unable to read from flash

1,419件の閲覧回数
anthony_bailey
Contributor I

I am using this as an IPMI chip and when I am sending a command to it we get a 0xD1 error stating "Command repsonse could not be provided. Device in firmware update mode." From what I can find it is something to do with reading from flash. Does anyone know what could cause this? Is there a pin shorted or something that shouldn't be?

ラベル(1)
0 件の賞賛
返信
1 返信

1,334件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Anthony Bailey,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Before answering your question, I'd like to know which type of command you use: ISP or IAP command.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信