LPC 2138 unable to read from flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC 2138 unable to read from flash

1,421 次查看
anthony_bailey
Contributor I

I am using this as an IPMI chip and when I am sending a command to it we get a 0xD1 error stating "Command repsonse could not be provided. Device in firmware update mode." From what I can find it is something to do with reading from flash. Does anyone know what could cause this? Is there a pin shorted or something that shouldn't be?

标签 (1)
0 项奖励
回复
1 回复

1,336 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Anthony Bailey,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Before answering your question, I'd like to know which type of command you use: ISP or IAP command.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复