LPC 1833 Timer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC 1833 Timer

1,652 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by akshaya.k55 on Wed Oct 14 02:21:59 MST 2015
Hi
I have a doubt in using timer module of LPC1833 32 bit ARM Cortex M3.
From the user guide i found like there are four timer modules timers 0/1/2/3 each having 4 channels.

Counter Mode:
I want to know if I can use all the four channels of all four timer modules at the same time.
That is, can this be used for 16 different timer inputs simultaneously?
Or only one channel at a time can be active?
I have this doubt because there is only one timer counter register present per timer module.

Timer Mode:
Configuring in timer mode, I want to measure 10 different time intervals simultaneously(i.e., starting instant same, ending instant different). Is this possible with the above chip?
标签 (1)
0 项奖励
回复
0 回复数